PROFINET Device4.2.0
 
Loading...
Searching...
No Matches
PN_API_IOD_SnmpLldpParams_t Struct Reference

SNMP parameters. More...

#include <pn_api_iod_types.h>

Data Fields

int8_t * pSysName
 
uint32_t sysNameLen
 
int8_t * pSysContact
 
uint32_t sysContactLen
 
int8_t * pSysLoc
 
uint32_t sysLocLen
 
int8_t * pSysDesc
 
uint32_t sysDescLen
 
int8_t * pIfDesc
 
uint32_t ifDescLen
 
int8_t * pPortName1
 
uint32_t portNameLen1
 

Detailed Description

SNMP parameters.