PROFINET Device4.2.0
 
Loading...
Searching...
No Matches
PN_API_IOD_Im0Data_t Struct Reference

IM0 Data structure. More...

#include <pn_api_iod_types.h>

Data Fields

uint16_t vendorId
 
uint8_t orderId [PN_API_IOD_IM0_ORDER_ID_LEN]
 
uint8_t serialNum [PN_API_IOD_IM0_SERIAL_NUM_LEN]
 
uint16_t hwRevision
 
PN_API_IOD_Im0SwRevision_t swRevision
 
uint16_t revisionCnt
 
uint16_t profileId
 
uint16_t profileSpecType
 
uint8_t versionMajor
 
uint8_t versionMinor
 
uint16_t imXSupported
 

Detailed Description

IM0 Data structure.