PROFINET Device4.2.0
 
Loading...
Searching...
No Matches
PN_API_IOD_Exp_t Struct Reference

Module/Submodule properties. More...

#include <pn_api_iod_types.h>

Data Fields

uint32_t arValid
 
uint32_t firstParamEndValid
 
uint32_t readyForInputUpdateValid
 
uint32_t numOfPluggedSubmods
 
uint32_t ioCrLen
 
uint32_t lastApduStatus
 
PN_API_IOD_ExpSubmod_t submod [PN_API_IOD_MAX_NUM_OF_SUBSLOTS]
 
uint32_t ioUpdatePending
 
uint16_t arType
 

Detailed Description

Module/Submodule properties.