PROFINET Device4.2.0
 
Loading...
Searching...
No Matches
PN_API_IOD_ErrState_t Struct Reference

#include <pn_api_iod_types.h>

Data Fields

uint8_t errCode
 
uint8_t errDecode
 
uint8_t errCode1
 
uint8_t errCode2
 
uint16_t addValue1
 
uint16_t addValue2
 

Detailed Description

  1. The first four parameters represent the PNIO Status. For details refer to IEC 61158-6 chapter 3.2.10.6 and 3.2.11.66.
  2. The last two parameters correspond to AdditionalValue1 and AdditionalValue2, see IEC 61158-6 chapter 3.2.11.50.
    The values shall contain additional user information within negative responses.
    The value zero indicates no further information.
    For positive read responses, the value 1 of the field AdditionalValue1 indicates that the Record Data Object contains more data than have been read.