Device annotation. More...
#include <pn_api_iod_types.h>
Data Fields | |
| int8_t | deviceType [PN_API_IOD_MAX_DEV_TYPE_LEN+1] |
| int8_t | orderId [PN_API_IOD_IM0_ORDER_ID_LEN+1] |
| int8_t | serialNum [PN_API_IOD_IM0_SERIAL_NUM_LEN] |
| uint16_t | hwRevision |
| int8_t | swRevisionPrefix |
| uint16_t | swRevision1 |
| uint16_t | swRevision2 |
| uint16_t | swRevision3 |
Device annotation.