Alarm data. More...
#include <pn_api_iod_types.h>
Data Fields | |
| uint16_t | arNum |
| uint16_t | sessionKey |
| uint32_t | api |
| uint16_t | slot |
| uint16_t | subslot |
| uint16_t | alarmPriority |
| uint16_t | alarmType |
| uint16_t | alarmSequence |
| bool | diagChannelAvailable |
| bool | diagGenericAvailable |
| bool | diagSubmodAvailable |
| uint8_t | reserved |
| bool | arDiagnState |
| uint32_t | modId |
| uint32_t | submodId |
| uint16_t | userStructId |
| uint16_t | userAlarmDataLen |
| uint8_t * | userAlarmData |
| uint32_t | cmPnioErr |
Alarm data.