PROFINET Device4.2.0
 
Loading...
Searching...
No Matches
PN_API_IOD_DevAddr_t Struct Reference

Module/Submodule address (logical/geographical). More...

#include <pn_api_iod_types.h>

Data Fields

PN_API_IOD_AddrType_t type
 
union { 
 
   uint32_t   addr 
 
   struct { 
 
      uint32_t   slot 
 
      uint32_t   subslot 
 
   }   geo 
 
address 
 

Detailed Description

Module/Submodule address (logical/geographical).