PROFINET Device4.2.0
 
Loading...
Searching...
No Matches
PN_API_IOD_ArInfo_t Struct Reference

AR information. More...

#include <pn_api_iod_types.h>

Data Fields

PN_API_IOD_ArType_t arType
 
uint32_t arNum
 
uint16_t arSessionKey
 
uint16_t sendClockFactor
 
uint16_t redRatioIoCrIn
 
uint16_t redRatioIoCrOut
 
uint32_t hostIp
 
uint32_t cycleFactor
 
uint16_t ppmEvent
 
uint16_t cpmEvent
 

Detailed Description

AR information.