| Id | Summary | Description |
|---|---|---|
| ICSTACK-442 | IO device requires a restart after cycle time adjustment by the PLC in IRT mode | In IRT mode, if the PLC changes the cycle time, the IO device needs to be restarted in order to restore it's correct functionality. This is causing "ShortCycles" testcase on Spirta to fail when the tester switches between 500us and 250us cycle time. |
| ARTTest-128 | SysRed S2 Part 2 - Scenario 3 | Bug in test bundle V2.44 and earlier. Fixed in test bundle V2.45 |
| ARTTest-129 | SysRed S2 Part 2 - Scenario 4 | Bug in test bundle V2.44 and earlier. Fixed in test bundle V2.45 |
| ARTTest-147 | MRP Interop - Client (CLRPC) | PLC program provided with the test bundle (version 2.44.4.2) is wrong. In order to pass this test, topology and MRP domain need to be changed. |
| ARTTest-228 to 233 | FSU - scenario 2 (CLRPC) | Complete scenario is pass with hint: Bug reported to pn-tester community https://pm-tsdg.profinet.com/issues/9111 |
| ARTTest-240 to 245 | FSU - scenario 4 (CLRPC) | Complete scenario is pass with hint: Bug reported to pn-tester community https://pm-tsdg.profinet.com/issues/9111 |
| ARTTest-317 | Manual-DHT test with 500us cycle time | When the PLC sets the cycle time to 500us and the DHT watchdog factor to 3, and a connection loss event appears in the network, the IO device sends the DHT expiry alarm with some extra delay. |