PROFINET Device4.2.0
 
Loading...
Searching...
No Matches
Introduction

This is the integration manual of the PROFINET® Device stack on Sitara™ AM263Px Platform. The PROFINET stack is executed on a dedicated R5F Core running FreeRTOS.

Note
The PROFINET stack could only be used with AM263Px type "F", usage with other chip types may be subject of faulty behavior!

The demo application was built with:

  • Code Composer Studio Version: 12.7.0
  • SysConfig v1.20.0
  • INDUSTRIAL-COMMUNICATIONS-SDK for AM263Px v09.02
  • TI Arm Clang Compiler 3.2.2.LTS

The latest testresult of the ART can be found here: art_testreport.pdf. The latest testresult of IRT Spirta (with a minimum of 500us cycle time) can be found here: spirta_testreport.pdf