PROFINET Device4.2.0
 
Loading...
Searching...
No Matches

◆ PN_APP_IOD_recordReadAsyncResponse()

void PN_APP_IOD_recordReadAsyncResponse ( void  )

Send asynchronous read response.

If asynchronous mode for read function is set to true, the user application is expected at one point to send a response to the request received earlier by PN_APP_IOD_cbRecordRead() function. The response is sent using this function. The function checks if there's any pending read request and sends its response.