Get the IM0 support of a submodule.
Based on its location, the IM0 support of a submodule is returned. The first submodule of slot 0 has device (DAP) info. The first submodule of any other slot has module info (virtual submodule interface).
- Parameters
-
| [in] | api | Application Process Identifier. |
| [in] | slot | Slot number. |
| [in] | subslot | Subslot number. |
| [in] | modId | Module identifier. |
| [in] | submodId | Submodule identifier. |
- Returns
- result of the operation as uint8_t
- Return values
-
| PN_API_IOD_Im0Support_t | IM0 support enum. |
- See also
- PN_API_IOD_Im0Support_t