PROFINET Device4.2.0
 
Loading...
Searching...
No Matches

◆ PN_APP_IOD_setIops()

void PN_APP_IOD_setIops ( uint32_t  slot,
uint32_t  subslot,
PN_API_IOD_IOXS  state 
)

Changes the IOPS value inside demoInDataIops global array.

Based on slot and subslot indexes, the IOPS value of the corresponding array element is changed.

Parameters
[in]slotSlot number.
[in]subslotSubslot index.
[in]stateIO provider state.
See also
PN_API_IOD_setIops