PROFINET Device4.2.0
 
Loading...
Searching...
No Matches

◆ PN_APP_IOD_cbArInData()

void PN_APP_IOD_cbArInData ( PN_API_IOD_Handle_t *const  pnHandle,
const uint16_t  arNum,
const uint16_t  sessionKey 
)

Callback function to inform that the cyclic data communication was started.

This function simply informs the user of this update.

Parameters
[in]pnHandleProfinet API Handle.
[in]arNumAR number.
[in]sessionKeySession key.
See also
PN_API_IOD_arInDataCbf