PROFINET Device4.2.0
 
Loading...
Searching...
No Matches

◆ PN_APP_IOD_updateAppCycle()

uint32_t PN_APP_IOD_updateAppCycle ( PN_API_IOD_Handle_t pnHandle,
uint32_t  timeNs 
)

Update App Cycle Timer.

This function updates the app cycletimer. The timer is by default configured in sysconfig.

Parameters
[in]pnHandleProfinet API Handle.
[in]timeNstimer interval in nanoseconds
Returns
result of the operation as uint32_t.
Return values
PN_API_OKSuccess.