PROFINET Device4.2.0
 
Loading...
Searching...
No Matches

◆ PN_APP_IOD_remaInit()

uint32_t PN_APP_IOD_remaInit ( void  )

Initialize ramNvData instance, load data from persistent memory and initialize the async write thread.

Returns
result of the operation as uint32_t.
Return values
PN_API_OKSuccess.
PN_API_NOT_OKSomething went wrong.