PROFINET Device4.2.0
 
Loading...
Searching...
No Matches

◆ PN_APP_IOD_cbDevAlarm()

void PN_APP_IOD_cbDevAlarm ( PN_API_IOD_Handle_t *const  pnHandle,
const PN_API_IOD_DevAlarmData_t devAlarmData 
)

Callback function to notify an alarm that has been received from the IO controller.

This function simply informs the user about the received alarm.

Parameters
[in]pnHandleProfinet API Handle.
[in]devAlarmDataPointer to alarm data.
See also
PN_API_IOD_devAlarmCbf