Functions and callbacks for the handling of IO device's alarms.
Functions | |
| void | PN_APP_IOD_cbAsyncReqDone (PN_API_IOD_Handle_t *const pnHandle, uint32_t arNum, PN_API_IOD_AlarmType_t alarmType, uint32_t api, PN_API_IOD_DevAddr_t *addr, uint32_t status, uint16_t diagnosisTag) |
| Callback function to acknowledge an asynchronous request (alarm) issued previously from the application to Profinet stack. | |
| void | PN_APP_IOD_cbDevAlarm (PN_API_IOD_Handle_t *const pnHandle, const PN_API_IOD_DevAlarmData_t *devAlarmData) |
| Callback function to notify an alarm that has been received from the IO controller. | |