PROFINET Device4.2.0
 
Loading...
Searching...
No Matches

◆ PN_API_IOD_RemaDataType_t

Type of remanent data.

Enumerator
PN_API_IOD_RemaDataMacAddr 

IO device's MAC address

PN_API_IOD_RemaDataDevName 

IO device's name

PN_API_IOD_RemaDataIpSuite 

IP suite (IP address, subnet mask, default router) in network format (big endian)

PN_API_IOD_RemaDataPdevRecord 

PDev records

PN_API_IOD_RemaDataIm1 

I&M1 data

PN_API_IOD_RemaDataIm2 

I&M2 data

PN_API_IOD_RemaDataIm3 

I&M3 data

PN_API_IOD_RemaDataIm4 

I&M4 data

PN_API_IOD_RemaDataSnmpSysName 

SNMP MIB2 object "system name"

PN_API_IOD_RemaDataSnmpSysCont 

SNMP MIB2 object "system contact"

PN_API_IOD_RemaDataSnmpSysLoc 

SNMP MIB2 object "system location"

PN_API_IOD_RemaDataPrivateData 

Own remanent data

PN_API_IOD_RemaDataArFsu 

UUID for AR-FSU functionality

PN_API_IOD_RemaDataSubmodCfg 

Submodule configurations

PN_API_IOD_RemaDataVendorParam 

Vendor parameter