#include "pn_api_iod_callbacks.h"
#include "pn_api_iod_settings.h"
#include "pn_api_iod_startup.h"
{...}
uint32_t status;
...}
PN_API_IOD_Handle_t * PN_API_IOD_new(void)
Creates Profinet API handle.
uint32_t PN_API_IOD_registerCallbacks(PN_API_IOD_Handle_t *const pnHandle, PN_API_IOD_Callbacks_t *callbacksInst)
Register callback functions.
PN_API_IOD_RtfOption_t
Reset To Factory option.
Definition pn_api_iod_types.h:310
struct PN_API_IOD_Handle PN_API_IOD_Handle_t
API handle instance which holds IO device's info.
Definition pn_api_iod_types.h:61
uint32_t PN_APP_IOD_cbResetToFactory(PN_API_IOD_Handle_t *const pnHandle, const PN_API_IOD_RtfOption_t rtfOption)
Callback function to reset IO device to factory settings.
PN_API_IOD_resetToFactoryCbf resetToFactory
Definition pn_api_iod_callbacks.h:45
Structure representing a set of callbacks.
Definition pn_api_iod_callbacks.h:41