#include "pn_api_iod_isoch.h"
uint32_t status;
uint32_t to;
uint8_t isrEventID = PN_API_IOD_TO_ISR_EVENT;
PN_API_IOD_Handle_t * PN_API_IOD_new(void)
Creates Profinet API handle.
uint32_t PN_API_IOD_activateIsoGpioObj(PN_API_IOD_Handle_t *const pnHandle, const uint32_t nsDelayTime, const uint32_t nsDurationTime, const uint8_t isomEvent)
Configures a comparator to generate a pulse on a chosen GPIO after/before a specified delay to a ne...
struct PN_API_IOD_Handle PN_API_IOD_Handle_t
API handle instance which holds IO device's info.
Definition pn_api_iod_types.h:61