PROFINET Device4.2.0
 
Loading...
Searching...
No Matches

◆ PN_API_IOD_isHandleValid()

bool PN_API_IOD_isHandleValid ( PN_API_IOD_Handle_t *const  pnHandle)

Check Profinet API handle validity.

The given handle has to be non-NULL and is has to be one of the previously allocated ones.

Parameters
[in]pnHandleProfinet API Handle.
Returns
result of the operation as bool.
Return values
trueHandle is valid.
falseHandle is invalid.
Example
#include "pn_api_iod_handle.h"
bool isValid = false;
isValid = PN_API_IOD_isHandleValid(pnHandle);
bool PN_API_IOD_isHandleValid(PN_API_IOD_Handle_t *const pnHandle)
Check Profinet API handle validity.
struct PN_API_IOD_Handle PN_API_IOD_Handle_t
API handle instance which holds IO device's info.
Definition pn_api_iod_types.h:61