PROFINET Device4.2.0
 
Loading...
Searching...
No Matches

◆ PN_API_IOD_init()

uint32_t PN_API_IOD_init ( PN_API_IOD_Handle_t *const  pnHandle)

Initializes Profinet stack.

The initialization process of the stack needs to have a handle that is previously created using PN_API_IOD_new().

Warning
Not implemented yet.
Parameters
[in]pnHandleProfinet API Handle.
Returns
result of the operation as uint32_t.
Return values
PN_API_OKSuccess.
PN_API_ERR_PARAMInvalid parameter.
Example
#include "pn_api_iod_handle.h"
uint32_t status;
pnHandle = PN_API_IOD_new();
status = PN_API_IOD_init(pnHandle);
PN_API_IOD_Handle_t * PN_API_IOD_new(void)
Creates Profinet API handle.
uint32_t PN_API_IOD_init(PN_API_IOD_Handle_t *const pnHandle)
Initializes Profinet stack.
struct PN_API_IOD_Handle PN_API_IOD_Handle_t
API handle instance which holds IO device's info.
Definition pn_api_iod_types.h:61