#include "pn_api_iod_handle.h"
uint32_t status;
PN_API_IOD_Handle_t * PN_API_IOD_new(void)
Creates Profinet API handle.
uint32_t PN_API_IOD_reset(PN_API_IOD_Handle_t *const pnHandle)
Resets Profinet stack.
uint32_t PN_API_IOD_run(PN_API_IOD_Handle_t *const pnHandle)
Runs Profinet stack.
uint32_t PN_API_IOD_init(PN_API_IOD_Handle_t *const pnHandle)
Initializes Profinet stack.
struct PN_API_IOD_Handle PN_API_IOD_Handle_t
API handle instance which holds IO device's info.
Definition pn_api_iod_types.h:61