Functions and callback-prototypes to control the handle of Profinet stack.
Functions | |
| PN_API_IOD_Handle_t * | PN_API_IOD_new (void) |
| Creates Profinet API handle. | |
| bool | PN_API_IOD_isHandleValid (PN_API_IOD_Handle_t *const pnHandle) |
| Check Profinet API handle validity. | |
| uint32_t | PN_API_IOD_delete (PN_API_IOD_Handle_t *const pnHandle) |
| Deletes Profinet API handle. | |
| uint32_t | PN_API_IOD_init (PN_API_IOD_Handle_t *const pnHandle) |
| Initializes Profinet stack. | |
| uint32_t | PN_API_IOD_run (PN_API_IOD_Handle_t *const pnHandle) |
| Runs Profinet stack. | |
| uint32_t | PN_API_IOD_reset (PN_API_IOD_Handle_t *const pnHandle) |
| Resets Profinet stack. | |
| uint32_t | PN_API_IOD_stop (PN_API_IOD_Handle_t *const pnHandle) |
| Stops Profinet stack. | |