#include "pn_api_iod_diagnostic.h"
#include "pn_api_iod_startup.h"
uint32_t status;
...
uint32_t api = 0;
uint16_t channelNum = 1;
uint16_t errorNum;
uint16_t diagTag = 1;
bool maintenanceReq = 1;
bool maintenanceDem = 0;
errorNum, chanDir, chanTyp, maintenanceReq, maintenanceDem, diagTag);
uint32_t PN_API_IOD_addDiagChannel(PN_API_IOD_Handle_t *const pnHandle, const uint32_t api, PN_API_IOD_DevAddr_t *const addr, const uint16_t channelNum, const uint16_t errorNum, const PN_API_IOD_DiagChannelPropDirection_t chanDir, const PN_API_IOD_DiagChannelPropType_t chanTyp, const bool maintenanceReq, const bool maintenanceDem, const uint16_t diagTag)
Add channel diagnostic alarm to PN stack.
PN_API_IOD_Handle_t * PN_API_IOD_new(void)
Creates Profinet API handle.
PN_API_IOD_DiagChannelPropType_t
Defines for channel properties.type.
Definition pn_api_iod_types.h:372
@ PN_API_IOD_DiagChannelPropTypeByte
Definition pn_api_iod_types.h:377
PN_API_IOD_DiagChannelPropDirection_t
Defines for channel properties.direction.
Definition pn_api_iod_types.h:359
@ PN_API_IOD_DiagChannelPropDirectionIn
Definition pn_api_iod_types.h:361
@ PN_API_IOD_AddrGeo
Definition pn_api_iod_types.h:155
struct PN_API_IOD_Handle PN_API_IOD_Handle_t
API handle instance which holds IO device's info.
Definition pn_api_iod_types.h:61
union PN_API_IOD_DevAddr_t::@0 address
PN_API_IOD_AddrType_t type
Definition pn_api_iod_types.h:446
struct PN_API_IOD_DevAddr_t::@0::@1 geo
uint32_t subslot
Definition pn_api_iod_types.h:453
uint32_t slot
Definition pn_api_iod_types.h:452
Module/Submodule address (logical/geographical).
Definition pn_api_iod_types.h:445