PROFINET Device4.2.0
 
Loading...
Searching...
No Matches

◆ PN_API_IOD_getRealSubmodList()

uint32_t PN_API_IOD_getRealSubmodList ( PN_API_IOD_Handle_t *const  pnHandle,
PN_API_IOD_RealSubmod_t **  realSubmodList,
uint32_t *  realSubmodListSize 
)

Gets information about real submodule list.

This function gets real submodule list information from the stack and returns a pointer to it to the user application.

Parameters
[in]pnHandleProfinet API Handle.
[out]realSubmodListSubmodule list to be returned.
[in]realSubmodListSizeSize of realSubmodList.
Returns
result of the operation as uint32_t.
Return values
PN_API_OKSuccess.
PN_API_NOT_OKSomething went wrong.
PN_API_ERR_PARAMInvalid parameter.
Example
#include "pn_api_iod_device.h"
#include "pn_api_iod_startup.h"
PN_API_IOD_Handle_t* pnHandle = NULL;
uint32_t status;
pnHandle = PN_API_IOD_new();
//Prepare and call PN_API_IOD_startup()
...
uint32_t realSubmodListSize = 0;
PN_API_IOD_RealSubmod_t *realSubmodList;
status = PN_API_IOD_getRealSubmodList(pnHandle, &realSubmodList, &realSubmodListSize);
uint32_t PN_API_IOD_getRealSubmodList(PN_API_IOD_Handle_t *const pnHandle, PN_API_IOD_RealSubmod_t **realSubmodList, uint32_t *realSubmodListSize)
Gets information about real submodule list.
PN_API_IOD_Handle_t * PN_API_IOD_new(void)
Creates Profinet API handle.
struct PN_API_IOD_Handle PN_API_IOD_Handle_t
API handle instance which holds IO device's info.
Definition pn_api_iod_types.h:61
Submodule information.
Definition pn_api_iod_types.h:813