#include "pn_api_iod_device.h"
#include "pn_api_iod_startup.h"
uint32_t status;
...
uint32_t api = 0, modId = 0x03010300, submodId = 0x31030004;
uint32_t inDataLen = 4, outDataLen = 0;
uint8_t iopsInitVal = 0;
submodId, inDataLen, outDataLen, im0Support, im0Data, iopsInitVal);
uint32_t PN_API_IOD_plugSubmod(PN_API_IOD_Handle_t *const pnHandle, uint32_t api, PN_API_IOD_DevAddr_t *addr, uint32_t modId, uint32_t submodId, uint32_t inDataLen, uint32_t outDataLen, uint8_t im0Support, PN_API_IOD_Im0Data_t *im0Data, uint8_t iopsInitVal)
Inserts a submodule into a subslot.
PN_API_IOD_Handle_t * PN_API_IOD_new(void)
Creates Profinet API handle.
@ PN_API_IOD_Im0Submodule
Definition pn_api_iod_types.h:72
@ PN_API_IOD_AddrGeo
Definition pn_api_iod_types.h:155
struct PN_API_IOD_Handle PN_API_IOD_Handle_t
API handle instance which holds IO device's info.
Definition pn_api_iod_types.h:61
union PN_API_IOD_DevAddr_t::@0 address
PN_API_IOD_AddrType_t type
Definition pn_api_iod_types.h:446
struct PN_API_IOD_DevAddr_t::@0::@1 geo
uint32_t subslot
Definition pn_api_iod_types.h:453
uint32_t slot
Definition pn_api_iod_types.h:452
Module/Submodule address (logical/geographical).
Definition pn_api_iod_types.h:445
IM0 Data structure.
Definition pn_api_iod_types.h:579