PROFINET Device4.2.0
 
Loading...
Searching...
No Matches

◆ PN_API_IOD_getRealSubmod()

uint32_t PN_API_IOD_getRealSubmod ( PN_API_IOD_Handle_t *const  pnHandle,
PN_API_IOD_RealSubmod_t **  realSubmod,
uint32_t  api,
uint32_t  slot,
uint32_t  subslot 
)

Gets real information about a submodule.

This function uses a submodule's API and address to get its real information from the stack and return a pointer to it to the user application.

Parameters
[in]pnHandleProfinet API Handle.
[out]realSubmodSubmodule structure to be returned.
[in]apiApplication Process Identifier.
[in]slotSlot number.
[in]subslotSubslot number.
Returns
result of the operation as uint32_t.
Return values
PN_API_OKSuccess.
PN_API_NOT_OKSomething went wrong.
PN_API_ERR_PARAMInvalid parameter.
Example
#include "pn_api_iod_device.h"
#include "pn_api_iod_startup.h"
PN_API_IOD_Handle_t* pnHandle = NULL;
uint32_t status;
pnHandle = PN_API_IOD_new();
//Prepare and call PN_API_IOD_startup()
...
uint32_t api = 0, slot = 1, subslot = 2;
status = PN_API_IOD_getRealSubmod(pnHandle, &realSubmod, api, slot, subslot);
uint32_t PN_API_IOD_getRealSubmod(PN_API_IOD_Handle_t *const pnHandle, PN_API_IOD_RealSubmod_t **realSubmod, uint32_t api, uint32_t slot, uint32_t subslot)
Gets real information about a submodule.
PN_API_IOD_Handle_t * PN_API_IOD_new(void)
Creates Profinet API handle.
struct PN_API_IOD_Handle PN_API_IOD_Handle_t
API handle instance which holds IO device's info.
Definition pn_api_iod_types.h:61
Submodule information.
Definition pn_api_iod_types.h:813