PROFINET Device4.2.0
 
Loading...
Searching...
No Matches

◆ PN_API_IOD_stopDevice()

uint32_t PN_API_IOD_stopDevice ( PN_API_IOD_Handle_t *const  pnHandle)

Stops communication with an IO device instance.

Halts all active Profinet connections. The IO device must first be initialized using either PN_API_IOD_openDevice() or PN_API_IOD_startup().

Parameters
[in]pnHandleProfinet API Handle.
Returns
result of the operation as uint32_t.
Return values
PN_API_OKSuccess.
PN_API_NOT_OKSomething went wrong.
PN_API_ERR_PARAMInvalid parameter.
Example
#include "pn_api_iod_device.h"
#include "pn_api_iod_startup.h"
PN_API_IOD_Handle_t* pnHandle = NULL;
uint32_t status;
pnHandle = PN_API_IOD_new();
//Prepare and call PN_API_IOD_startup()
...
status = PN_API_IOD_stopDevice(pnHandle);
uint32_t PN_API_IOD_stopDevice(PN_API_IOD_Handle_t *const pnHandle)
Stops communication with an IO device instance.
PN_API_IOD_Handle_t * PN_API_IOD_new(void)
Creates Profinet API handle.
struct PN_API_IOD_Handle PN_API_IOD_Handle_t
API handle instance which holds IO device's info.
Definition pn_api_iod_types.h:61