#include "pn_api_iod_data.h"
uint32_t status, arNum = 1, apduStatus = 0;
...
...
uint32_t PN_API_IOD_initiateDataRead(PN_API_IOD_Handle_t *const pnHandle)
Initiates data read in Profinet stack and Performs one-time exchange of IO output data between the us...
uint32_t PN_API_IOD_getLastApduStatus(PN_API_IOD_Handle_t *const pnHandle, const uint32_t arNum, uint32_t *const apduStatus)
Gets the Application Protocol Data Unit (APDU) status of the output data.
PN_API_IOD_Handle_t * PN_API_IOD_new(void)
Creates Profinet API handle.
struct PN_API_IOD_Handle PN_API_IOD_Handle_t
API handle instance which holds IO device's info.
Definition pn_api_iod_types.h:61