PROFINET Device4.2.0
 
Loading...
Searching...
No Matches

◆ PN_API_IOD_freeRemaMemCbf

typedef uint32_t( * PN_API_IOD_freeRemaMemCbf) (PN_API_IOD_Handle_t *const pnHandle, uint8_t *const destMem)

Callback function prototype to request to clear data from NV memory.

This function is called by Profinet stack to request from the user application to free Profinet-related data from the NV memory.

Parameters
[in]pnHandleProfinet API Handle.
[in]destMemPointer to a buffer where the data to be cleared.
Returns
result of the operation as uint32_t.
Return values
PN_API_OKSuccess.
PN_API_ERR_PARAMInvalid parameter.
Example
#include "pn_api_iod_bsp.h"
#include "pn_api_iod_callbacks.h"
#include "pn_api_iod_startup.h"
//Implement the callback function in the user application
PN_API_IOD_Handle_t *const pnHandle,
uint8_t *const destMem)
{...}
PN_API_IOD_Handle_t* pnHandle = NULL;
uint32_t status;
pnHandle = PN_API_IOD_new();
//Store callback functions implemented by the user application
...}
//Register callback function
status = PN_API_IOD_registerCallbacks(pnHandle, &callbacks);
PN_API_IOD_Handle_t * PN_API_IOD_new(void)
Creates Profinet API handle.
uint32_t PN_API_IOD_registerCallbacks(PN_API_IOD_Handle_t *const pnHandle, PN_API_IOD_Callbacks_t *callbacksInst)
Register callback functions.
struct PN_API_IOD_Handle PN_API_IOD_Handle_t
API handle instance which holds IO device's info.
Definition pn_api_iod_types.h:61
uint32_t PN_APP_IOD_cbFreeRemaMem(PN_API_IOD_Handle_t *const pnHandle, uint8_t *const destMem)
Callback function to request to clear remanent data from NV memory.
PN_API_IOD_freeRemaMemCbf freeRemaMem
Definition pn_api_iod_callbacks.h:48
Structure representing a set of callbacks.
Definition pn_api_iod_callbacks.h:41