PROFINET Device4.2.0
 
Loading...
Searching...
No Matches

◆ PN_API_IOD_setLedCbf

typedef uint32_t( * PN_API_IOD_setLedCbf) (PN_API_IOD_Handle_t *pnHandle, PN_API_IOD_Led_t led, bool state)

Callback function prototype to request changing of LED states.

This function is called by Profinet stack if a LED need to change its state.

Parameters
[in]pnHandleProfinet API Handle.
[in]ledPort number (currently not used).
[in]stateBlinking frequency in Hz.
Returns
result of the operation as uint32_t.
Return values
PN_API_OKSuccess.
Example
#include "pn_api_iod_bsp.h"
#include "pn_api_iod_callbacks.h"
#include "pn_api_iod_startup.h"
//Implement the callback function in the user application
PN_API_IOD_Handle_t *const pnHandle,
PN_API_IOD_Led_t led, bool state)
{...}
PN_API_IOD_Handle_t* pnHandle = NULL;
uint32_t status;
pnHandle = PN_API_IOD_new();
//Store callback functions implemented by the user application
...}
//Register callback function
status = PN_API_IOD_registerCallbacks(pnHandle, &callbacks);
PN_API_IOD_Handle_t * PN_API_IOD_new(void)
Creates Profinet API handle.
uint32_t PN_API_IOD_registerCallbacks(PN_API_IOD_Handle_t *const pnHandle, PN_API_IOD_Callbacks_t *callbacksInst)
Register callback functions.
PN_API_IOD_Led_t
Type for LEDs.
Definition pn_api_iod_types.h:108
struct PN_API_IOD_Handle PN_API_IOD_Handle_t
API handle instance which holds IO device's info.
Definition pn_api_iod_types.h:61
uint32_t PN_APP_IOD_cbSetLed(PN_API_IOD_Handle_t *const pnHandle, const PN_API_IOD_Led_t led, const bool state)
Callback function to set LED states.
PN_API_IOD_setLedCbf setLed
Definition pn_api_iod_callbacks.h:49
Structure representing a set of callbacks.
Definition pn_api_iod_callbacks.h:41