PROFINET Device4.2.0
 
Loading...
Searching...
No Matches

◆ PN_API_IOD_devAlarmCbf

typedef void(* PN_API_IOD_devAlarmCbf) (PN_API_IOD_Handle_t *const pnHandle, const PN_API_IOD_DevAlarmData_t *devAlarmData)

Callback function prototype to notify an alarm that has been received from the IO controller.

This function sends the received alarm information to the user application.

Parameters
[in]pnHandleProfinet API Handle.
[in]devAlarmDataPointer to alarm data.
Example
#include "pn_api_iod_alarm.h"
#include "pn_api_iod_callbacks.h"
#include "pn_api_iod_startup.h"
//Implement the callback function in the user application
PN_API_IOD_Handle_t *const pnHandle,
{...}
PN_API_IOD_Handle_t* pnHandle = NULL;
uint32_t status;
pnHandle = PN_API_IOD_new();
//Store callback functions implemented by the user application
...}
//Register callback function
status = PN_API_IOD_registerCallbacks(pnHandle, &callbacks);
PN_API_IOD_Handle_t * PN_API_IOD_new(void)
Creates Profinet API handle.
uint32_t PN_API_IOD_registerCallbacks(PN_API_IOD_Handle_t *const pnHandle, PN_API_IOD_Callbacks_t *callbacksInst)
Register callback functions.
struct PN_API_IOD_Handle PN_API_IOD_Handle_t
API handle instance which holds IO device's info.
Definition pn_api_iod_types.h:61
void PN_APP_IOD_cbDevAlarm(PN_API_IOD_Handle_t *const pnHandle, const PN_API_IOD_DevAlarmData_t *devAlarmData)
Callback function to notify an alarm that has been received from the IO controller.
Alarm data.
Definition pn_api_iod_types.h:755
PN_API_IOD_devAlarmCbf devAlarm
Definition pn_api_iod_callbacks.h:66
Structure representing a set of callbacks.
Definition pn_api_iod_callbacks.h:41