#include "pn_api_iod_alarm.h"
uint32_t status, api = 0, userHandle = 0;
uint8_t buf[64];
uint8_t bufSize = 64:
uint16_t ident = 0;
uint32_t PN_API_IOD_sendProcessAlarm(PN_API_IOD_Handle_t *const pnHandle, const uint32_t api, PN_API_IOD_DevAddr_t *const addr, uint8_t *const data, const uint32_t dataSize, const uint16_t identUserStruct, const uint32_t userHandle)
This function notifies the IO controller of a process alarm unique to this submodule.
PN_API_IOD_Handle_t * PN_API_IOD_new(void)
Creates Profinet API handle.
@ PN_API_IOD_AddrGeo
Definition pn_api_iod_types.h:155
struct PN_API_IOD_Handle PN_API_IOD_Handle_t
API handle instance which holds IO device's info.
Definition pn_api_iod_types.h:61
union PN_API_IOD_DevAddr_t::@0 address
struct PN_API_IOD_DevAddr_t::@0::@1 geo
uint32_t subslot
Definition pn_api_iod_types.h:453
uint32_t slot
Definition pn_api_iod_types.h:452
Module/Submodule address (logical/geographical).
Definition pn_api_iod_types.h:445