#include "pn_api_iod_alarm.h"
uint32_t status, api = 0, userHandle = 0;
addr.address.geo.subslot = 0;
uint32_t PN_API_IOD_sendRetOfSubAlarm(PN_API_IOD_Handle_t *const pnHandle, const uint32_t api, PN_API_IOD_DevAddr_t *const addr, const uint32_t userHandle)
The function sends a “Return of Submodule” alarm to the IO controller. The alarm is triggered when th...
PN_API_IOD_Handle_t * PN_API_IOD_new(void)
Creates Profinet API handle.
@ PN_API_IOD_AddrGeo
Definition pn_api_iod_types.h:155
struct PN_API_IOD_Handle PN_API_IOD_Handle_t
API handle instance which holds IO device's info.
Definition pn_api_iod_types.h:61
union PN_API_IOD_DevAddr_t::@0 address
struct PN_API_IOD_DevAddr_t::@0::@1 geo
uint32_t slot
Definition pn_api_iod_types.h:452
Module/Submodule address (logical/geographical).
Definition pn_api_iod_types.h:445