This structure is used for the Scan Status List. More...
#include <IOLM_SMI_Types.h>
Data Fields | |
| INT16U | u16ArgBlockID |
| Big endian. | |
| INT8U | u8ScanStatus |
| Scan status. | |
| INT8U | u8ScanResults |
| Number of scan results (max 255). | |
| IOLM_SMI_SScanStatusResult | asResult [128] |
| array of scan results | |
This structure is used for the Scan Status List.
The ArgBlockID(IOLM_SMI_EArgBlockID) for this struct is IOLM_SMI_eArgBlockID_WScanStatusList = 0x9201.