IO-Link Master2.02.03
 
Loading...
Searching...
No Matches
IOLM_SMI_SWMasterConfigListOld Struct Reference

This structure is obsolete. It used for the wireless Master configuration before V1.1.3 release. More...

#include <IOLM_SMI_Types.h>

Data Fields

INT16U u16ArgBlockID
 Big endian.
 
INT8U u8MasterID
 1 - 29.
 
INT8U u8AHTEnable
 0 = disabled, 1 = enabled.
 
INT8U au8Blocklist [10]
 
INT16U u16PairingTimeout
 Pairing timeout in seconds.
 

Detailed Description

This structure is obsolete. It used for the wireless Master configuration before V1.1.3 release.

The ArgBlockID(IOLM_SMI_EArgBlockID) for this struct is IOLM_SMI_eArgBlockID_WMasterConfig = 0x0200.