IO-Link Master2.02.03
 
Loading...
Searching...
No Matches
IOLM_SMI_SScanStatusResult Struct Reference

This structure is used for a single scan result. More...

#include <IOLM_SMI_Types.h>

Data Fields

INT8U u8ResSlotType
 Slot type.
 
INT8U au8ResUniqueID [9]
 Unique ID.
 
INT8U u8ResRevID
 Revision ID.
 

Detailed Description

This structure is used for a single scan result.