IO-Link Master2.02.03
 
Loading...
Searching...
No Matches
IOLM_SMI_SPortConfigList Struct Reference

This structure is used to store port configuration. More...

#include <IOLM_SMI_Types.h>

Data Fields

INT16U u16ArgBlockID
 Big endian.
 
INT8U u8PortMode
 See IOLM_SMI_EPortMode.
 
INT8U u8ValidationBackup
 See IOLM_SMI_EValidationBackup.
 
INT8U u8IQBehavior
 See IOLM_SMI_EIQBehavior.
 
INT8U u8PortCycleTime
 
INT16U u16VendorID
 Big endian.
 
INT32U u32DeviceID
 Big endian.
 

Detailed Description

This structure is used to store port configuration.

The ArgBlockID(IOLM_SMI_EArgBlockID) for this struct is IOLM_SMI_eArgBlockID_PortConfigList = 0x8000.