IO-Link Master2.02.03
 
Loading...
Searching...
No Matches
IOLM_SMI_SInstance Struct Reference

Data Fields

INT8Upu8MasterIdentification
 
INT16U u16MasterIdentLength
 
IOLM_SMI_SJob asuJobs [8 *4]
 
IOLM_SMI_SJobList suEmptyQueue
 
IOLM_SMI_SJobList suGeneralQueue
 
IOLM_SMI_SPortInstance asuPort [8]
 
INT32U u32NvAlignmentDummy
 
IOLM_SMI_SNVConfiguration suNvConfiguration
 
TBOOL boNvConfigChanged
 
TBOOL boNVSaveInProgress
 
INT32S s32TickValNvSave
 Tick to limit frequency of save to EEPROM operations.
 
INT32S s32TickValMaintenance
 Tick for maintenance actions.
 
INT8U u8MaintenancePort
 
INT8U u8DSPort
 
INT8Upu8DSData
 If not NULL there is a waiting storage.
 
INT16U u16DSLength
 
TBOOL boDSInProgress