IO-Link Master2.02.03
 
Loading...
Searching...
No Matches
IOLM_SMI_SHeader Struct Reference

SGI dependent types. More...

#include <IOLM_SMI_Types.h>

Data Fields

INT8U u8Service
 IOLM_SMI_EServiceID.
 
INT8U u8Reserved
 Reserved.
 
INT16U u16ExpRefArgBlockId
 Expected response or referenced ArgBlock Id in big endian.
 
INT8U u8Instance
 Addressed instance (port, track, etc.).
 
INT8U u8ClientId
 Client id. IOLM_SMI_CLIENTID_INTERN and IOLM_SMI_CLIENTID_BROADCAST are reserved.
 
INT16U u16ArgBlockLength
 Little endian.
 

Detailed Description

SGI dependent types.

This structure is used for the SMI_Header.

The SMI_Header is sent before every data exchange to prepare the recipient for the following data. On serial transmission after the Header follows an ArgBlock with u16ArgBlockLength number of bytes.