This structure is used to store FS port configuration. More...
#include <IOLM_SMI_Types.h>
Data Fields | |
| INT16U | u16ArgBlockID |
| Big endian. | |
| INT8U | u8PortMode |
| INT8U | u8ValidationBackup |
| INT8U | u8IQBehavior |
| INT8U | u8PortCycleTime |
| INT16U | u16VendorID |
| Big endian. | |
| INT32U | u32DeviceID |
| Big endian. | |
| INT16U | u16FSPTime2Ready |
| INT16U | u16FSPMinShutDownTime |
| INT32U | u32FSCPAuthenticity1 |
| INT32U | u32FSCPAuthenticity2 |
| INT8U | u8FSPPort |
| INT16U | u16FSPAuthentCRC |
| INT8U | u8FSPProtVersion |
| INT8U | u8FSPProtMode |
| INT16U | u16FSPWatchdogTime |
| INT16U | u16FSPIOStructCRC |
| INT32U | u32FSPTechParCRC |
| INT16U | u16FSPProtParCRC |
| INT8U | u8IODescVersion |
| INT8U | u8SPDUInLength |
| INT8U | u8TotalOfInBits |
| INT8U | u8TotalOfInOctets |
| INT8U | u8TotalOfInInt16 |
| INT8U | u8TotalOfInInt32 |
| INT8U | u8SPDUOutLength |
| INT8U | u8TotalOfOutBits |
| INT8U | u8TotalOfOutOctets |
| INT8U | u8TotalOfOutInt16 |
| INT8U | u8TotalOfOutInt32 |
This structure is used to store FS port configuration.
The ArgBlockID(IOLM_SMI_EArgBlockID) for this struct is IOLM_SMI_eArgBlockID_FSPortConfigList = 0x8100.