IO-Link Master2.02.03
 
Loading...
Searching...
No Matches
IOLM_SMI_SFSPDIn Struct Reference

This structure is used for FS Process Data input and output read back. More...

#include <IOLM_SMI_ExtTypes.h>

Data Fields

INT16U u16ArgBlockID
 Big endian.
 
INT8U u8SDset
 Safe data settings applied.
 
INT8U u8Faults
 Faults.
 
INT8U u8OperatorAckRequest
 Operator acknowledge request.
 
INT8U u8FSInputDataLength
 
INT8U au8FSData [25]
 Input data length in bytes.
 

Detailed Description

This structure is used for FS Process Data input and output read back.

The ArgBlockID(IOLM_SMI_EArgBlockID) for this struct is IOLM_SMI_eArgBlockID_FSPDIn = 0xB101.

Field Documentation

◆ au8FSData

INT8U IOLM_SMI_SFSPDIn::au8FSData[25]

Input data length in bytes.

25 bytes FS PD.