IO-Link Master2.02.03
 
Loading...
Searching...
No Matches
IOLM_SGI_SClient Struct Reference

SMI client information. More...

#include <IOLM_SGI.h>

Data Fields

INT8U u8ClientId
 Cleint Uniuqe ID.
 
INT8U u8IsRegistered
 
INT32U u32ClientRights
 
IOLM_SGI_SClientName sClientName
 The name of the client.
 
IOLM_SMI_CBGenericCnf cbCallback
 
IOLM_SGI_SPortDescriptor sPortDecs [8]
 the registered callbacks
 

Detailed Description

SMI client information.

structure contains the information to a smi client

Field Documentation

◆ sPortDecs

IOLM_SGI_SPortDescriptor IOLM_SGI_SClient::sPortDecs[8]

the registered callbacks

<

a structure with the port rights