IO-Link Master2.02.03
 
Loading...
Searching...
No Matches
IOLM_SDSObject Struct Reference

This structure defines Data Storage objects. More...

#include <IOLM_Types.h>

Data Fields

INT8U au8Index [2]
 
INT8U u8Subindex
 
INT8U u8Length
 
INT8U au8Data [4]
 

Detailed Description

This structure defines Data Storage objects.

The structure can be used on non aligned buffer. Because of this, there are only byte values defined. The data field is only a dummy value and it's real length depends on the content.