IO-Link Master2.02.03
 
Loading...
Searching...
No Matches
IOL_SDirectParam1 Struct Reference

This structure stores the Direct Parameter Page 1. More...

#include <IOL_Types.h>

Data Fields

INT8U u8MasterCommand
 
INT8U u8MasterCycleTime
 
INT8U u8MinCycleTime
 
INT8U u8MSequenceCapability
 
INT8U u8RevisionID
 
INT8U u8ProcessDataIn
 
INT8U u8ProcessDataOut
 
INT8U u8VendorID1
 
INT8U u8VendorID2
 
INT8U u8DeviceID1
 
INT8U u8DeviceID2
 
INT8U u8DeviceID3
 
INT8U u8FunctionID1
 
INT8U u8FunctionID2
 
INT8U u8Reserved
 
INT8U u8SystemCommand
 

Detailed Description

This structure stores the Direct Parameter Page 1.