IO-Link Master2.02.03
 
Loading...
Searching...
No Matches
Data Structures
Here are the data structures with brief descriptions:
 CIOL_SDirectParam1This structure stores the Direct Parameter Page 1
 CIOL_SEventEntryThis structure defines a event buffer entry
 CIOLM_DataLogThis structure is used for data logging
 CIOLM_DataLogDownlinkThis structure is used for downlink logging
 CIOLM_DataLogUplinkThis structure is used for uplink logging
 CIOLM_FW_SFWUHeaderThis structure is used for firmware downloads
 CIOLM_FW_SFWUSegmentThis structure is used for firmware downloads
 CIOLM_SDSContentThis structure defines the Data Storage content
 CIOLM_SDSObjectThis structure defines Data Storage objects
 CIOLM_Settings_RFThis structure is used for settings of the RF chips
 CIOLM_SGI_GatewayManagerIdent
 CIOLM_SGI_SClientSMI client information
 CIOLM_SGI_SClientManagerSMI client manager information
 CIOLM_SGI_SPortDescriptorSMI client name struct
 CIOLM_SGI_STimerEventDescSMI client name struct
 CIOLM_SMasterCfgThis structure is used for the stack configuration
 CIOLM_SMI_SArgBlockParamThis structure follows the IOLM_SMI_SHeader struct
 CIOLM_SMI_SCallbacksSMI Callbacks. Must be initialized via IOLM_SMI_vInit
 CIOLM_SMI_SDataLogThis structure is used for stack information
 CIOLM_SMI_SDeviceEventThis structure is used for Device Events (remote)
 CIOLM_SMI_SDSDataThis structure is used for DataStorage Data
 CIOLM_SMI_SFirmwareThis structure is used for firmware transfer
 CIOLM_SMI_SFSCPAuthenticityThis structure is used to retrieve FSCPAuthenticity
 CIOLM_SMI_SFSMasterAccessThis structure is used to get FS Master access
 CIOLM_SMI_SFSPDInThis structure is used for FS Process Data input and output read back
 CIOLM_SMI_SFSPDInOutThis structure is used for FS Process Data input and output read back
 CIOLM_SMI_SFSPDOutThis structure is used for FS Process Data output
 CIOLM_SMI_SFSPortConfigListThis structure is used to store FS port configuration
 CIOLM_SMI_SHeaderSGI dependent types
 CIOLM_SMI_SInstance
 CIOLM_SMI_SJob
 CIOLM_SMI_SJobErrorThis structure is used as JobError ArgBlock
 CIOLM_SMI_SJobList
 CIOLM_SMI_SMasteridentThis structure is used to get Master identification
 CIOLM_SMI_SNVConfiguration
 CIOLM_SMI_SOnRequestDataThis structure is used for On-request Data
 CIOLM_SMI_SPDInThis structure is used for Process Data input
 CIOLM_SMI_SPDInIQThis structure is used for IQ input
 CIOLM_SMI_SPDInOutThis structure is used for Process Data input and output read back
 CIOLM_SMI_SPDOutThis structure is used for Process Data output
 CIOLM_SMI_SPDOutIQThis structure is used for IQ output
 CIOLM_SMI_SPortConfigListThis structure is used to store port configuration
 CIOLM_SMI_SPortEventThis generic structure is used for events
 CIOLM_SMI_SPortEventThis structure is used for port events (local)
 CIOLM_SMI_SPortInstance
 CIOLM_SMI_SPortPowerOffOnThis structure is used for PortPowerOffOn requests
 CIOLM_SMI_SPortStatusListThis structure is used to store port status
 CIOLM_SMI_SScanResultThis structure is used for scan results
 CIOLM_SMI_SScanStatusResultThis structure is used for a single scan result
 CIOLM_SMI_SSettingsThis structure is used for settings transfer
 CIOLM_SMI_SSPDUInThis structure is used for SPDU input
 CIOLM_SMI_SSPDUOutThis structure is used for SPDU output
 CIOLM_SMI_SStackInformationThis structure is used for stack information
 CIOLM_SMI_SStdHeader
 CIOLM_SMI_STestCommandThis structure is used for Kunbus regression test support
 CIOLM_SMI_SVoidArgBlockThis structure is used as general and void ArgBlock
 CIOLM_SMI_SWMasterConfigListOldThis structure is obsolete. It used for the wireless Master configuration before V1.1.3 release
 CIOLM_SMI_SWPairingListThis structure is used to trigger a pairing request
 CIOLM_SMI_SWPortConfigListThis structure is used for the wireless port configuration
 CIOLM_SMI_SWPortConfigListOldThis structure is obsolete. It used for the wireless port configuration before V1.1.3 release
 CIOLM_SMI_SWPortStatusListThis structure is used to store wireless port status
 CIOLM_SMI_SWScanConfigListThis structure is used to trigger a scan request
 CIOLM_SMI_SWScanStatusListThis structure is used for the Scan Status List
 CIOLM_SMI_SWSingleScanStatusListThis structure is used for the Scan Status List of a single scan result
 CIOLM_SMI_SWTrackConfigListThis structure is used for the track configuration
 CIOLM_SMI_SWTrackStatusListThis structure is used to store track status
 CIOLM_SMI_V113_SWPortStatusListThis structure is used to store wireless port status in V1.1.3
 CIOLM_SMsgHandlerConfigThis structure stores the message handler configuration
 CIOLM_SPageRequestThis structure stores the data of a page request
 CIOLM_SPDBufferThis structure is used for Process Data buffer handling
 CIOLM_SPDBufferCtrl
 CIOLM_SPortConfigThis structure is used for the desired port mode
 CIOLM_SRealPortConfigThis structure is used for the actual used communication parameters