EtherNet/IP™ Adapter3.09.00
 
Loading...
Searching...
No Matches
EI_API_ADP_UIntfConf Union Reference

Structure to use as function parameter (attribute parameters) More...

#include <EI_API_def.h>

Data Fields

uint8_t all
 
EI_API_ADP_SIntfConfBits_t bit
 

Detailed Description

Structure to use as function parameter (attribute parameters)