EtherNet/IP™ Adapter3.09.00
 
Loading...
Searching...
No Matches
EIP_SLoadParameter Struct Reference

#include <EI_API_ADP_define.h>

Data Fields

uint8_t ai8uMacAddr [EIP_MAC_ADDR_LEN]
 
uint32_t pruIcssCfgId
 
PRUICSS_ConfigPtr pPruIcssCfg
 
uint32_t * pPru0Firmware
 
uint32_t pPru0FirmwareLength
 
uint32_t * pPru1Firmware
 
uint32_t pPru1FirmwareLength
 
ETHPHY_ConfigPtr pEthPhyCfg [2]
 
ETHPHY_Handle ethPhyHandle [2]
 
bool mdioManualMode
 
uint32_t mdioManualModeBaseAddress
 
uint32_t * pMdioManualModeFirmware
 
uint32_t mdioManualModeFirmwareLength
 
uint32_t mdioManualModeFirmwareConfig
 
OSAL_TASK_Priority_t taskPrioPhyMdixTask